How can we help you today?

EPE for ASP Library: The graphic “Label” is hidden in runtime on OMI view app

The labels can be seen for the GPL instances by two method
1. Use the GPL layout template(LayoutGP) for displaying the runtime information
2. Use the "PSXlabels" object as one of the panes in the configured layout
This means If the customer uses any Layout templates other than GPL needs to use the "PSXlabels" objects as one of the panes as explained below
For example customer uses the WWD_L_Desktop layout
1. Navigate to the WWD_L_Desktop from the graphic tool box
2. Edit the same and add a pane where user wants to place the "PSXlables" object
3. Search the "PSXlables" object in the toolbox and drag the same to the respective pane. check the below pic
4. Save the changes and preview the changes



Schneider Electric Saudi Arabia