Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Uninstalling Eclipse in Ubuntu
RemoteConnect 3.0.3 works with Eclipse version 2022-06 for the SDK on the Edge platform

If a customer is having issues with Eclipse and needs to repair/reinstall it or if they have an incorrect version installed that needs to be removed.

From a terminal window in Ubuntu (Ctl-Alt-T)

cd ~/
rm -rf ./eclipse
rm -rf ./.eclipse
rm -rf ./oecore-i686/

This will remove all of the components associated with Eclipse. Please refer to the SCADAPack x70 Documentation "Installing Eclipse and SCADAPack 47xi SDK" for reinstalling Eclipse and the SDK.