How can we help you today?

How do you downgrade the libset version of a Control Expert project?

Issue
Libset version downgrade

Environment
EcoStruxure Control Expert

Resolution
There may be a time where you are running a new Control Expert version than someone else. If someone is using a older Control Expert version they will not have the new libset and will not be able to open the project. In this case you can accommodate the older version by downgrading the libset version with these steps:

1. Have your Control Expert project opened and built.
2. Save the project as an archived. File -> Save Archive...
3. Within Control Expert initiat the opening of the archive file.
4. Navigate to the file but hold off opening until you select the option at the bottom of the explorer window to specify libset version.
5. Select the appropriate libset version then open the project.
6. Rebuild the project and it will now have the older libset version.

Schneider Electric Saudi Arabia