Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which cables are required for a Lexium P Robot optional module?
These cables are required for each motor of the module:
  • VW3E2098Rxxx (Encoder cable) + VW3E2100Rxxx (Encoder extension cable)
  • VW3E1166Rxxx (Power cable) + VW3E1168Rxxx (Power extension cable)

Rotational Modules:
  • VRKPXYYYYY00045
  • VRKPXYYYYY00046
Tilting Modules:
  • VRKPXYYYYY00053
Double Rotational Modules:
  • VRKPXYYYYY00038
  • VRKPXYYYYY00049
Additional information to: Lexium P Robot - Hardware Guide - Optional Equipment