How can we help you today?

EcoStruxure Control Expert - What are the READ_STS_MX Limitations?

Product line
EcoStruxure Control Expert

Description
The block READ_STS_MX has the same limitations as the READ_VAR because it uses TCP/IP, when you use a READ_VAR you have to manage execution to your EF managing the reports, depending on the CPUs type or connection point EFs numbers in // can change.

image

Then you can use add an unlimited number of blocks to logic, but you must execute them sequentially or not exceed the number of simultaneous connections.

Here is a short example: How to know the absence of x80 IO in local M580 rack when it is configured as Device DDT ?

Schneider Electric Saudi Arabia