When ION8650 firmware versions were released?
Issue
When were different versions of firmware for IO8650 meter released?
Product
ION8650
Resolution
Please refer to the following table for release dates of ION8650 firmware.
Please note that not all versions of firmware are available from Schneider Electric website se.com.
When were different versions of firmware for IO8650 meter released?
Product
ION8650
Resolution
Please refer to the following table for release dates of ION8650 firmware.
| Firmware Version | Release Date |
|---|---|
| V004.040.001 | January 2021 |
| V004.031.002 | August 2019 |
| V004.031.001 | April 2019 |
| V004.031.000 | November 2018 |
| V004.021.002 | November 2017 |
| V004.021.000 | April 2017 |
| V004.020.001 | March 2015 |
| V409 | February 2015 |
| V408 | November 2014 |
| V407 | July 2014 |
| V406 | March 2014 |
| V405 | August 2013 |
| V404 | April 2013 |
| V403 | March 2012 |
| V402 | June 2011 |
Please note that not all versions of firmware are available from Schneider Electric website se.com.
Released for: Schneider Electric Saudi Arabia