How can we help you today?

What is the meaning of Yellow State Color in Control Expert 16.0 Status Bar

Yellow state in the status BAR for all information:

Modification of the memory state (depending on the memory fragmentation state). In BUILT state:

built

Connected to the Simulator:

simulator

In not built state:

not built

UDE APi interface with Read Only mode:

server

Safety state:

Partial RUN for SAFETY applications (RUN Safe or RUN Proc)

A yellow colored status is meaning something is not correct.

·       PROCESS Task RUN (At least one) - SAFE task STOP -> RUN in yellow

·       PROCESS Tasks in STOP (All)    - SAFE task RUN -> RUN in yellow

run

Maintenance mode :

maintain

No Upload information:

upload

Schneider Electric Saudi Arabia