Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Guidelines for Engineering Client Configuration

Issue

Guideline for Configuring Engineering Clients


Product Line

Power Monitoring Expert 7.2x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment

Engineering Client
Primary PME Server


Resolution

Engineering clients require several settings to be configured in order to communicate with the primary PME server and SQL database.

  • The base PME license includes 1 Engineering client license for the primary server, additional licenses are required for additional clients
  • A standalone server or an application server must be installed before installing an Engineering client.
  • Engineering Clients require that the Power Monitoring Expert folder on the PME server is shared with full read and write permissions. File and Printer Sharing must be enabled.


Additional guidelines can be found in the attached PDF. Installation instructions can be found in the PME system guide. PME 2023 System Guide - PME Installation Instructions

Schneider Electric Saudi Arabia

Attachment(s)
10 Steps - Extra guidelines deploying Engineering clients.pdf [503.43 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre