Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to have a specific K1/K2 camswitch IP65 ?

Article available in these languages: French

The standard delivery is IP40 for K1/K2

Witrh configurator, it is possible to select a gasket (KZ73) in accessories but only for multifixing operating heads with 45X45 front plate (you need to select a label)

For front mounting, the configurator software doesn't propose IP accessories

--> For front plate 45X45, as the reference KZ65 is canceled, I suggest to order it through generic reference GCR_K1S + technical text KZ65

--> For front plate 60X60, the reference KZ66 is still commercialized. It can be ordered separately.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: