Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Machine SCADA Expert, Como Box Object and Array Tags.

Issue:

Combo Box object using an Array Tag as the Data Source:

When the screen is viewed on the runtime server, the Combo Box displays the selection list correctly.

Combo Box list on runtime server

But when viewed on a Thin Client, the Combo Box only displays the first element of the list or Array Tag.

Combo Box list through Mobile Access

Product Line:

EcoStruxure Machine SCADA Expert (all versions)

Resolution:

In the Help document of EcoStruxure Machine Expert, under the Combo Box object , for the Data Source Type: Array tag,

It is mentioned: This type is not supported in project screens that are viewed through Mobile Access. (This includes Thin Clients.)

It is needed to use another Data Source Type.

Combo Box object help section

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre