How can we help you today?

How to load an M172 project with a USB memory stick?

  1. The power to the M172 should be turned off (no connections to the USB mini port for programming).
  2. Insert the USB stick and then apply power.
  3. At boot-up the M172 will detect the USB memory stick and will copy the project from the USB device into the PLC.
  4. When the copy process is finished only the Green LED on the M172 will be lit.
  5. Remove USB memory stick and then power cycle the M172 PLC.
  6. The new program will begin operating.

Modicon M172 Logic Controller Hardware Guide

Schneider Electric Saudi Arabia
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
Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Centre

Help Centre

Find support resources for all your needs, in one place.

  • Product Documentation