How can we help you today?

The MC function blocks returns an error when using them with the ATV320.

The reason the issue occurs is because the MC functions blocks do not support the ATV320.  The MC function blocks only supports legacy drives (i.e, ATV32, etc.)

The issue can be resolved by updating to firmware 2.9IE34 which includes a new parameter to disguise the ATV320 as an ATV32.

regtg

wgt

rwgtr

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre