1.Context
In certain conditions, it could happen that the installation of the SchneiderPLCUSBDriverSuite finish without error and getting the message that the driver is well installed like on the following screenshot.
However, the PLC USB Driver can’t be seen inside the driver manager :
Even inside the program and features of windows :
2. How to solve
To solve this problem, please follow the step below :
- Stop ‘NetAccess Service’ in Services manually.
- Delete C:\windows\System32\UsbConnect.exe , If you can’t delete it, rename it as other name.
- Re-install the SchneiderPLCUSBDriverSuite.exe.
3. Product
SchneiderPLCUSBDriverSuite
4. Environment
Windows 10 and above
Released for: Schneider Electric Saudi Arabia