How can we help you today?

What are the ring tip sizes included with the CP12142LI?

Issue:

What are the ring tip sizes included with the CP12142LI?

Product Line:

Back-UPS Connect CP12142LI

Environment:

All Serial Numbers

Cause:

Customers are asking as ring tip sizes are not indicated in the user manual or technical specification.

Resolution:

***  All measurements are in mm ***

TIP 1M Black/Green 5.5*2.5*12 L

TIP 5.5*2.0 Jack

TIP 1F Black/Black 5.5*2.0*12 L

TIP 5.5*2.5 Jack

TIP 2M Black/Green 5.5*2.5*12 L

TIP 6.5*3.0 Jack

TIP 2F Black/Black 6.5*3.0*12 L

TIP 5.5*2.5 Jack

Note:

  • Although CP12142LI’s compatibility is not limited to the listed AT&T™ modem/routers as listed in the Compatibility and Runtimes document , end users are encouraged to check with their modem or router's manufacturer to ensure that their device works with the CP12142LI output specs (12VDC, 3.2A) and ring tip size.

Should there be any further concerns, please contact our Customer Care Center at https://www.apc.com/us/en/support/

Schneider Electric Saudi Arabia