How can we help you today?

Why the usage of Batch files ofsservice.bat and ofsnoservice.bat is not available anymore in OFS version 3.63 SP3 ?

The usage of batch files ofsservice.bat (resp. ofsnoservice.bat) may be vulnerable and are no more installed.

Solution :

Run instead regofsservice /true (resp. regofsservice /false) in a command line to register (resp. unregister) the server as a service.

Product line :

OFS 3.63 SP3

Environment :

Windows 10 and above

Schneider Electric Saudi Arabia