Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can an ATV900 Frame Size 7 be installed without a DC Choke?

Issue:
Can you install an ATV900 Frame Size 7 without a DC Choke?

Product Line:
Altivar 900 series Frame Size 7

Environment:
All serial numbers for Altivar 900 Series Frame Size 7

Cause:
N/A

Resolution:

You need to add a jumper between PO and PA+ when installing the drive without a DC Choke.

PA & PO Terminals

Note:

For ATV930 products that have no DC choke, a line reactor is necessary to be installed.