Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
HDPM6000 head unit is not displaying current readings

Issue

The HDPM6000 head unit is not reading current even though the CT's are wired to the unit.

Product Line

HDPM6000

Resolution

The HDPM6000 head unit requires voltage connections as well as current connections in order to read properly.  If only CT's are connected, the unit will not display values for current.  Voltage must also be connected to the unit in order for the current to be read.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre