Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
could we compare the inrush current of the PLC "M580"/"Premium" power supplies?

Some customers are surprised by the inrush current values of the DC power supplies for M580 BMXCPS4022, BMXCPS4022S, and BMXCPS3020.

This can cause problems with energy distribution limitations for customers using 10 or 100 power supplies.

For each product in our catalog, we have provided the features "I²t," "It," and "inrush current." This allows users to select the appropriate circuit breaker.

When we connect multiple PLCs to a single power line, the inrush current generates a voltage drop for a few milliseconds. Our PLC power supplies are designed to withstand these brief voltage drops. However, some other devices may be disturbed by these short voltage drops, so clients need to organize power distribution accordingly.

We are working to improve the "inrush current" feature in our future power supplies.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: