Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the internal power consumption of the Schneider OffGrid Portable Power Station when turned off or not in use?

Issue:

What is the internal power consumption of the Schneider OffGrid Portable Power Station when turned off or not in use?


Product Line:

Schneider OffGrid Portable Power Station

Environment:

All serial numbers

Resolution:

With the system turned off after 1 hr. (when LCD is off & no output is on), the power consumption in this state is under 0.5mA.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: