Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a timer in EcoStruxure Control Expert that counts up and also counts down?

Issue:
Timer in EcoStruxure Control Expert that shows the timer counting up and also counting down


Product Line:
EcoStruxure Control Expert


Resolution:
EcoStruxure Control Expert does not natively have a timer that counts down. All the standard timer blocks only count up. Attached is a DFB that shows the timer counting up and counting down.

Schneider Electric Saudi Arabia

Attachment(s)
TIMER_COUNT_UP_DOWN.zip [954 Bytes]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre