How can we help you today?

Clearances for installing a PrismaSeT I switchboard in a room

Inside a switchboard there is heat dissipation from the devices and busbars in a normal running condition. This heat is dissipated out of switchboard mainly through the air circulation inside the switchboard by means of convection.

PrismaSeT I has rear panels which has louvers on top and bottom for an IP30/42 solution. These louvers allow the cold air to enter the switchboard from the bottom, absorb heat from switchboard, rise up and goes out through the top louver.

image 1

Incase of IP54 solution, this is taken care by forced ventilation

image 2

For this airflow to happen, it is essential the a gap is maintained between the switchboard and walls/roof while installation. Hence back to back assembly is not recommended with PrismaSeT I.

While installing a switchboard in a room it is recommended to maintain clearances for the reasons mentioned.

  • free space to enable for complete opening of the doors and operator access, maintenance or using a lifting device
  • Provide at least 600 mm of free space above PrismaSeT for incoming cable from top.
  • Sufficient space from rear of the panel to wall for the heat dissipation from the switchboard.

Also, recommendations from local regulations shall be taken care.

Schneider Electric Saudi Arabia