Shrouds for GS2 Product line
Issue: Terminal shrouds do not fit GS2 lugs.
Product Line: GS2 Product line
Environment: GS2 Lugs and Shrouds
Resolution:
The Terminal shrouds for the GS2 product line was designed to work with crimp style lugs only. We have had positive results in the past using them with single pole lug kits such as GS1AW403 however they do not work in conjunction with any multipole kits such as the power distribution lugs
Currently there is no project on the backlog to create shrouds specific for the power distribution lugs or double pole lugs for the GS2 range.
Released for: Schneider Electric Saudi Arabia