Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
SRTG UPS Reports Self-Test Refused After a Successful Self-Test

Problem: The self-test status of SRTG UPS models reports "Refused" after a successful self-test

ref

Product Line: UPS models with the prefix SRTG

Cause: Due to the current firmware logic, it is expected behavior that SRTG UPS models report "Refused" after a successful self-test. The expected self-test status sequence is Status: In Progress -> Actual self-test screen -> Status: Refused, as shown below:

prog -> prog -> red

Resolution: A future firmware update will improve the UPS self-test reporting.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: