IGP10-T 4 and 20 mA Loop Check
- Press the NEXT button 3 times and CALIB will be displayed
- Press ENTER and CAL ATO will be displayed
- Press NEXT 3 times and ADJ 4mA will be displayed
- Press ENTER and A 4mAΔΔ will be displayed. At this time the transmitter output will be locked at 4mA.
- When 4mA loop check is done, press NEXT 5 times and ADJ20mA will be displayed
- Press ENTER and A20mAΔΔ will be displayed. At this time the transmitter output will be locked at 20mA.
- When 20mA loop check is done, press NEXT 6 times and CANCEL will be displayed
- Press ENTER and transmitter will return to measurement mode.
Released for: Schneider Electric Saudi Arabia
Discontinued
Discontinued