How can we help you today?

What is the maximum number of subroutines that can be configured in a EcoStruxure Control Expert project?

Issue:

Max number of subroutines in a project

Product Line:

EcoStruxure Control Expert

Resolution:

A maximum of 64 subroutines can be programmed in the LD, FBD, IL or ST language

Schneider Electric Saudi Arabia