How can we help you today?

How to Install a Smart UPS Ultra Modular into a 2-Post Rack

Issue:
Installation of a Smart UPS Ultra Modular into a 2-post rack

Product Line:
Smart UPS Ultra Modular 1PH

Environment:
All serial numbers (Global)

Resolution:

The following Photo is the Safety Warning Alert for UPS installation

NOTE: The 2 post mounting brackets (SRYLOPT2 for mounting UPS Frame and SRYLOPT5 for mounting the XBP frame) are available as an accessory and should be procured separately.

The APC Smart-UPS Modular Ultra, an Uninterruptible Power Supply (UPS), is designed for easy installation in a 2-post mount.

Models With UPS Frames Only:

Image below shows step 1 for Smart-UPS Ultra Modular 2-post rack installation Image below shows step 2 for Smart-UPS Ultra Modular 2-post rack installation

Image below shows step 3 for Smart-UPS Ultra Modular 2-post rack installation Image below shows step 4 for Smart-UPS Ultra Modular 2-post rack installation

Image below shows step 5 for Smart-UPS Ultra Modular 2-post rack installation Image below shows step 6 for Smart-UPS Ultra Modular 2-post rack installation

Models with both UPS and battery frames

Image below shows step 1 for Smart-UPS Ultra Modular with Extended Battery Frame in a 2-post rack installation Image below shows step 2 for Smart-UPS Ultra Modular with Extended Battery Frame in a 2-post rack installation

Image below shows step 3 for Smart-UPS Ultra Modular with Extended Battery Frame in a 2-post rack installation Image below shows step 4 for Smart-UPS Ultra Modular with Extended Battery Frame in a 2-post rack installation

Image below shows step 5 for Smart-UPS Ultra Modular with Extended Battery Frame in a 2-post rack installation Image below shows step 6 for Smart-UPS Ultra Modular with Extended Battery Frame in a 2-post rack installation

Image below shows step 7 for Smart-UPS Ultra Modular with Extended Battery Frame in a 2-post rack installation Image below shows step 8 for Smart-UPS Ultra Modular with Extended Battery Frame in a 2-post rack installation

Image below shows step 9 for Smart-UPS Ultra Modular with Extended Battery Frame in a 2-post rack installation Image below shows step 10 for Smart-UPS Ultra Modular with Extended Battery Frame in a 2-post rack installation

You may also  refer to the attached manual (refer to page 23 onwards).

If you have any clarifications and/or requests for the above mentioned available information, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.

Schneider Electric Saudi Arabia

Attachment(s)
EN 990-6492D.pdf [3.43 MB]