Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to access the web interface of APC by Schneider Electric Dry Contact I/O (AP9614)

Topic:

How to access the web interface of APC by Schneider Electric Dry Contact I/O (AP9614)

Product Line:
AP9614

Environment:
All serial number (Global)

Resolution:

The APC by Schneider Electric has released last  Jan. 20, 2025 its new Dry Contact I/O card (AP9614). Below are the steps on how to connect on the AP9614 Dry Contact I/O card :

Note: Although the manual states that the AP9614 Dip Switch must be set to Config 4, the web will still be accessible even if set to other Dip Switch Configuration. Refer to FAQ000273842.

1. Connect to the AP9614 Dry Contact I/O card by using supplied USB cable and a computer that is capable of NDIS eg. Windows 10 or higher, Linux. Note: Max of 15ft distance is tested.

The image shows a computer trying to connect to a Micro USB cable  to a Dry Contact I/O AP9614

2. Once connected, kindly confirm if the "Remote NDIS Compatible Device" under Network Adapters is showing. If not, you may want to consider checking a missing driver on your computer, wrong USB cable used or contacting your vendor.

The image shows Remote NDIS Compatible was recognized under Network Adapters in Device Manager.

2. Use a web browser to access the http://169.254.111.222 (NOTE:- https is not supported).

The image shows accessibility of AP9614 via http:169.254.111.222

3. Login to the card with the default user name and password (apc/apc).

4. Change the password when prompted at the first login.

5. Access the card and enter apc in the user name box and the new password that you had configured.

6. You may now continue to set configuration if Dip Switch is  set to Configuration 4.

If you have any clarifications and/or requests for the above mentioned available information, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: