How to Extract Data in SBUS server?
Title
How to extract data using SBUS server?
Issue
Data is needed outside of EPAS application, for example, technical analysis, reporting, data archival, etc.
Product Line
EcoStruxure Power Automation System (EPAS)
EcoStruxure Microgrid Operation (EMO)
PACiS
EcoSUI
Environment
SBUS Server
Resolution
- Open SBUS server application > select the Extraction tab
- Select measurements to be extracted by either:
- Selecting individually using the Select Signals window (click save to create a .lst file for repetitive use)
- Select 'Load' to import a list file (.lst)
- Select dates for the desired time period > Extract. NOTE: Depending on dates selected and number of signals, files can be quite large.
4. Select the directory where you'd like to store the extraction file and select Save.