How can we help you today?

Smart UPS Ultra - Experiences a System Braindead / Battery Pack Is Not Compatilble

Problem:

  • Battery Pack is not compatible
  • P08, P11, P16 and P19 alarms (pre-charger damage)
  • G03 alarm (logic power supply alarm)
  • System Brain Dead
  • Battery lost communication



Product Line: SRTL3KRM1UWC, SRTL3KRM1UIC, SRTL2K2RM1UWC, SRTL2K2RM1UIC, SRTL3KRM1UC, SRTL2K2RM1UC, SRTL3KRM1UWNC, SRTL3KRM1UINC, SRTL2K2RM1UWNC, SRTL2K2RM1UINC, SRTL3KRM1UNC, SRTL2K2RM1UNC

Environment: All Serial Numbers

Cause

The power factor correction (PFC) circuit is experiencing sagging current at higher input voltages (>240VAC), leading to defects in logic power and causing the system to become brain dead. Additionally, battery timing and traffic congestion are contributing to system mismatches

Resolution:

Firmware ID1062 and ID1063 v4.9 has been released and addresses this issue as well as the following

1. Improve PFC sagging current when input voltage is larger than 240V.
2. Reduce input peak current at on‐line transient moment when input voltage is larger than 240V.
3. When a fault is detected during self‐test, prevent turning on PFC and transfer to failure bypass mode.
4. Force battery to sleep while UPS is in fault to avoid consuming battery energy.
5. Adjust the fan control algorithm for reducing noise.

The firmware can be downloaded here - https://download.schneider-electric.com/files?p_Doc_Ref=Smart-UPS_FW_Release_Notes&p_enDocType=Firmware&p_Archive_Name=Smart-UPS_FW_Release_Notes.zip

Schneider Electric Saudi Arabia