OFS (OPC Factory Server) Error 1053: The service did not respond to the start or control request in a timely fashion
Issue
Error 1053: the service did not respond to the start or control request in a timely fashion is displayed when attempting to start/restart the OFService.
Product Line
OFS
OPC Factory Server
Environment
Windows Services
Cause
OFService is failing to start within a specified amount of time
Resolution
- In the Windows search bar look up Services, right-click, and run as Administrator
- find the service where the error occurred, right-click on it, and Select Properties
- In the Properties window, click the Log On tab
- Make sure the "This Account" option is selected and enter the username and password for the account with administrator privileges
- click the Apply button, then click the OK button
- Restart your computer and check if the service has started successfully
Released for: Schneider Electric Saudi Arabia