Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which HMI models are no longer supported in Vijeo Designer version 6.3 compared to version 6.2?

Issue

Not able to download to the HMI because it is not showing as a Target in Vijeo Designer v6.3

Product Line

Vijeo Designer v6.3

Resolution

Vijeo Designer version 6.3 no longer supports certain legacy HMI models that were previously compatible with version 6.2, as these models have been officially discontinued.

Below is a list of HMI model families that are no longer supported in Vijeo Designer version 6.3:

-HMISTO

-XBTGK

-XBTGT (all series)

-Various iPCs:

Compact MPC

Compact PC BOX

Flex PC BOX

HMIGTW

S-BOX PC (HMIBSO and HMIBSU)

Smart BOX

Smart/Smart+ MPC

XBTGTW