How can we help you today?

Is TM3 Haz Loc Certification meaning Class I Div 2 ?

Issue:

Is Haz Loc Certification of TM3 meaning Class I Division 2 environments?

Product Lines:

TM3 modules

Environment:

All model numbers

Resolution:

Yes, The Haz Loc Certification means approval for using in explosive environment Class I Div2.

This is a certification from UL, in file E361380. UL logo, together with Class I, Division 2, Group ABCD and this File number is also marked on the product.

Schneider Electric Saudi Arabia