Replacement for ZBRN1
Title: Replacement for ZBRN1
Issue: What is the replacement product for the ZBRN1?
Product Line: ZBRN1
Environment: Harmony Hub
Resolution:
The suggested replacement for the Harmony Hub ZBRN1 is the Panel Server line product references:
PAS400
PAS600*
PAS800*
PAS gateways are compatible with ZBRT* transmitters from frimware version 002.002.000. The latest version is published on the website and can be downloaded by customers.
Note: Hardware version should be taken into account as well (HW V1 or HW V2 depends on the gateway type).
User guide: EcoStruxure Panel Server User Guide
Released for: Schneider Electric Saudi Arabia