Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ETE - FAQ - Offer: Can I trust EcoStruxure Transformer Expert technology?

The technology was built upon a foundation of over a decade of research conducted by the University of Queensland researchers, collaborating with four of Australia’s largest distribution and transmission utilities. It is based on peer-reviewed research and is verified by testing and data gathered from a large number of transformers.

Academic papers describing the methodology and white papers explaining the use of the EcoStruxure Transformer Expert methodology are available in Academic Papers.