How can we help you today?

ETE - FAQ - Logger: Is EcoStruxure Transformer Expert Sensor weatherproof?

The sensor is IP67 rated. The body of the sensor is made from aluminum and powder coated green, while the probe is made from stainless steel.
Both aluminum and stainless steel offers natural protection against corrosion.

Schneider Electric Saudi Arabia