How are the ATV320 Function Block Identification Fbi- parameters used?
Response:
Understanding Fbi-
These parameters are populated as Function Block Logic is added to the ATV320 Logic Configuration in software like SoMove:
For Example:
BVER is the Program Version:
BNS is the Program Size:
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Released for: Schneider Electric Saudi Arabia