Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the structure of Canalis for EV capable of withstanding environmental loads typical in snow-prone region?

The KEV structural system is engineered to withstand a snow load of up to 90 kg/m² and to resist wind speeds up to 210 km/h.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: