Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is CPU over-clocking with Turbo-boost available for PSA6?

Yes, the default setting is Turbo-boost enabled. It can be disabled from the BIOS menu.

When Turbo-boost is turned on for PSA6 with Core i5 CPU, it is recommended to use a power supply with at least 80% higher capacity than the specified power consumption.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre