How do I resolve the "The Control Expert certificate is missing. Open Security Editor on the local computer and enroll Control Expert software" error when I launch Control Expert V16.0 and above?
Issue:
Error message "The Control Expert certificate is missing. Open Security Editor on the local computer and enroll Control Expert software"
Product Line:
Ecostruxure Control Expert
Resolution:
Follow the steps below to create a new certificate?
- Launch the security editor tool
2. click on the certificate action tab and click on generate self signed certificate. Afterwards try to open control expert.
Username: SecurityAdmin
Uassword: Azertyuiop123456789!