How can we help you today?

TGML - Breakers Will Not Update Status

Issue

Breakers will not update status on the WebHMI when the breaker status physically or virtually changes.

Product Line

Power Scada Operation 2020

Power Scada Operation 2020 R2

Power Scada Operation 2021

Ecostruxure Power Operation 2022

Ecostruxure Power Operation 2024

Environment

Graphics Editor

WebHMI

Cause

Some component libraries (including SAG libraries as of 2021) require the use of global scripts. Many modern components have had scripts removed from them and rely on the functionality of the global script. UseGlobalScripts should be set to True in order to take advantage of these changes.

Resolution

  1. Under the TGML object, set UseGlobalScripts field to True.
    1. UseGlobalScripts Field
  2. Make sure that each bind field is using the fully qualified item name (Cluster.Name.ItemTag).
    1. Fully Qualified Item Name for Bind fields

Schneider Electric Saudi Arabia