How to control an ATV Drive using a HMIST6 with Modbus TCP?
Issue
Trying to control an ATV Drive with an HMIST6 without using a PLC via Modbus TCP
Product Line
HMIST6 HMI Family
ATV Drives Family
Environment
SoMove
EcoStruxure Operator Terminal Expert
Resolution
A) ATV Drive Setup in SoMove
1. On the SoMove project assign a Fixed IP address.
2. Set a Drive Modbus Address, it can be 1. If more than one drive is being used, make sure every drive has a different address number.
3. Set the protocol configuration to "Modbus TCP" if there is more than one protocol option.
4. Set the control mode configuration CHCF to "I/O mode".
B) HMI Setup in EOTE
1. Add a Modbus TCP Master driver.
2. Set the IP address and Equipment Address to match the configuration on the ATV Drive.
3. Under variables, add the variables manually. Use the Logic Address information that matches the ATV Drive being used.
Example:
4. Bind the variables to the screen objects.
5. Download the projects and test.
Released for: Schneider Electric Saudi Arabia