How can we help you today?

SCADAPack Configuration software and Corresponding Controllers

SCADAPack devices are configured and programmed using a variety of specialized software tools. Each tool serves a unique purpose, from ladder logic programming to advanced configuration and diagnostics.

Primary Software Platforms

  • SCADAPack Workbench
    A comprehensive development environment supporting multiple programming languages including C++, ISaGRAF (IEC 61131-3), and Relay Ladder Logic.

  • SCADAPack Configurator
    Used for configuring SCADAPack 330, 334 models, and SCADAPack 32 with ISAGRAF firmware.

  • SCADAPack E Configurator
    Tailored for SCADAPack E-series devices, offering enhanced configuration capabilities.

  • Telepace Studio
    A programming tool supporting Relay Ladder Logic, widely used for SCADAPack 300 series and SCADAPack 32.

  • Remote Connect and Control Expert
    Advanced tools for remote diagnostics, configuration, and control of SCADAPackx70 RTUs.

  • Target 3 & Target 5
    These refer to specific firmware environments used for programming and deploying applications on SCADAPack devices.

The tableshowing which SCADA Pack software tools support which hardware models.

Software ToolSupported SCADAPack Models Supported SCADAPack Models
SCADAPack workbenchTarget 3SCADAPack 100SCADAPack 314SCADAPack 32(5601)SCADAPack 32(5604)SCADAPack 32(5606)SCADAPack 32PSCADAPack 330SCADAPack 334SCADAPack 350SCADAPack 350V1SCADAPack 357SCADAPack 357V1SCADAPack 4203 DRSCADAPack 4203 DS
Target 5SCADAPack 300ESCADAPack 500ESCADAPack ES/ER
SCADAPack ConfiguratorSCADAPack 100.1024KSCADAPack 314SCADAPack 32SCADAPack 32PSCADAPack 330SCADAPack 334SCADAPack 350SCADAPack 4203 DRSCADAPack 4203 DS
SCADAPack E ConfiguratorSCADAPack 500ESCADAPack 535ESCADAPack ES Model ASCADAPack ES Model BSCADAPack ES Model CSCADAPack ER-P600SCADAPack ER-P620SCADAPack 312ESCADAPack 313ESCADAPack 314ESCADAPack 300ESCADAPack 333ESCADAPack 334ESCADAPack 337ESCADAPack 350ESCADAPack 357E
Telepace StudioMicro 16SCADAPackSCADAPack LightSCADAPack PlusSCADAPack 100.256KSCADAPack 100.1024KSCADAPack LPSCADAPack 314SCADAPack 32SCADAPack 32PSCADAPack 330SCADAPack 334SCADAPack 350SCADAPack 4203 DRSCADAPack 4203 DSSCADAPack 4202 DRSCADAPack 4202 DSFlowStation 100NOC60
Remote Connect and Control ExpertSCADAPack 474SCADAPack 474iSCADAPack 470SCADAPack 470iSCADAPack 570SCADAPack 574SCADAPack 575

Note:

  1. Both the Serck 386 and 586 eNETs used the E Series Configurator and E Series Firmware (hence will work with either ISaGRAF for E Series, or SCADAPack Workbench for E Series).
  2. Serck 586 was re-named as SCADAPack ES at one point.

Schneider Electric Saudi Arabia