What is our Salt Spray rating on a QED-2 Switchboard?
Subject:
Verification of QED2 Switchboard Paint Finish Standards
Issue:
Paint Standard – Humidity and Corrosion Resistance Testing
Product Line:
QED2 Switchboard
Environment:
Replacement Projects / Product Evaluation
Cause:
Product Design and Material Specifications
Resolution:
• Please refer to the attached PDF document, which includes the technical cut sheet for the paint used in QED2 switchboards.
• The document outlines the results of the 1,000-hour salt spray test, demonstrating compliance with corrosion resistance standards.
• This information can be used to verify finish durability in humid or corrosive environments.