How can we help you today?

Ecostruxure Process Expert for ASP[2023]: How to configure the user login for SequenceGP block

This knowledge base explains the user on the steps to configure the security user for SequenceGP template.

By default, the SequenceGP template in the ASP runtime operates without user login, as the security setting for the attribute named SeqCtl.St.Command.PV is configured to FreeAccess.

Image_1

To enable security for operating the Sequence template, the user must update the security settings of the SeqCtl.St.Command.PV attribute as shown below.

Image_2

This is applicable till EPEFASP2023 + ASP2023R2SP1 version.

Schneider Electric Saudi Arabia