Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Retrieve Maintenance Log from PowerLogic P5 Relay

Article available in these languages: Spanish

Issue:

Need to obtain the internal maintenance log file from an PowerLogic P5 relay for troubleshooting or analysis.

Product:

PowerLogic P5 Protection Relay

Environment:

  • PowerLogic P5 relay
  • Latest eSetup Easergy Pro software (downloadable from Schneider Electric website)
  • PC connected to the relay via front USB port
  • Relay powered off (HMI should display “5V USB only”)

Cause:

Maintenance logs are stored internally in the relay and require specific steps and credentials to access.

Resolution:

1.-Download and install the latest eSetup Easergy Pro software from Schneider Electric’s website.

2.- Ensure the relay is not powered on. Connect the P5 relay to the PC using the front USB port.

1

3.- Wait until the relay HMI displays “5V USB only”.

4.- In Easergy Pro, click Read Maintenance Log File.

2

5.- Log in using the following credentials:

Login: InstallerLevel

Password: AAAA

3

6.- Save the log file to your desired location. The file will have the extension .p5I.

4

7. - Send the .p5I file to the Advance Tech support team for further analysis.

5

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre