Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to extract COMTRADE data from High-End Platform - HEP meters (PM8000, ION7400, and ION 9000) and ION8650 meter using ION Setup?

Issue

There is no available guide for extracting COMTRADE data from meters with that capability, and no relevant information could be found in the meter documentation.

Product Line

HEP Meters(PM8000, ION7400, and ION 9000)

ION8650

ION Setup

Environment

Configuration

Cause

The users would like to extract the COMTRADE Data on the meters with that capability.

Resolution

Not all our meters support the COMTRADE feature. Only the ION8650 and the High-End Platform (HEP) meters—PM8000, ION7400, ION 9000 include this capability. While there may be other methods to extract COMTRADE data from these meters, the ION Setup software can also be used for this purpose.

Below is a step-by-step procedure for extracting COMTRADE data using ION Setup.

  1. On High-End Platform meters – HEP: PM8000, ION7400, and ION 9000 or ION8650 meter
  • Download and install the latest version of the ION Setup software and firmware on your laptop or PC.
  • Add the meter to ION Setup when the meter is connected to a laptop or PC directly or from the Network
  • Then click on the meter  > Double click on Setup Assistant  > Power quality > Sag/Swell Logging > Select the records > Save > Select the period > OK.

Fig. 01

Figure 01

Fig. 02

Figure 02

Fig. 03

Figure 03

The following message will appear if the is no COMTRADE data during the period selected above.

Fig. 04

Figure 04

By changing the period, from

Fig. 05

Figure 05

Fig. 06

Figure 06

  1. On ION8650
  • Download and install the ION Setup Software in a Laptop or PC
  • Add the meter to ION Setup when the meter is connected to a Laptop or PC directly or from the Network
  • Then click on the meter  > Double click on Setup Assistant  > Power quality > COMTRADE > Select the Data files needed (Sag/Swell, Sag/Swell Depth, Transient Status, or Transient Depth) > Save > Select the period > OK

Fig. 07

Figure 07

Fig. 08

Figure 08

Fig. 09

Figure 09

Fig. 10

Figure 10

Fig. 11

Figure 11

Fig. 12

Figure 12

Fig. 13

Figure 13

Then double click on each file and select the file format needed to save or view the data.

  1. Documentation:

Schneider Electric Saudi Arabia

Explore more
Range:
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre