How can we help you today?

Application Notes for PowerLogic P3 Protection Relays

Issue

Users need guidance on where to find technical application notes for PowerLogic P3 devices covering protocols, configuration, and maintenance.

Product

PowerLogic P3 Protection Relay

Environment

Utility substations, industrial automation systems, and environments using PowerLogic P3 relays for protection and communication.

Cause

Difficulty locating official Schneider Electric documentation for advanced features such as RSTP, Ethernet/IP, DeviceNet, Modbus, IEC 61850, and protection settings.

Resolution

Application notes for Powerlogic P3 devices are available through Schneider Electric’s official documentation portal. Key files include:

  • P3APS17002EN – Rapid Spanning Tree Protocol (RSTP)
  • P3APS17003EN – Ethernet/IP configuration instructions
  • P3APS17004EN – Parallel Redundancy Protocol for Easergy P3
  • P3APS17007EN – DeviceNet configuration instructions
  • P3APS17008EN – DeviceNet and EtherNet/IP data model
  • P3APS17013EN – Current transformer selection
  • P3APS17014EN – Recommended maintenance activities
  • P3APS17016EN – Restricted earth fault protection
  • P3APS18025EN – Modbus configuration
  • P3APS18026EN – Logic Editor
  • P3APS19001EN – IEC 61850 configuration instructions
  • P3APS19027EN – Directional phase overcurrent protection

To access these documents:

  1. Visit Schneider Electric’s web page, Go to the menu path Support > Product Documentation & Software > All Documents and Software.
  2. Search using the file name or keywords (e.g., “PowerLogic P3 RSTP” or “IEC 61850 configuration”).
  3. Download the PDF for detailed instructions.

Or you can go directly from the next link (active as Nov 25): Here

Schneider Electric Saudi Arabia