Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to generate a list of DNP3 Generic or Modbus - Advanced Generic Direct Outstations with their IP Addresses - Single Network

It might be helpful, for maintenance purposes, to have a list of outstations with their respective IP Addresses. Below are two queries that can be used to generate such lists for DNP3 Generic points and Modbus – Advanced Generic Direct Outstations, respectively:

SELECT

O.ID, O.FULLNAME, N.ADDRESS

FROM

CDNP3OSDIRECT AS O CROSS JOIN CSINGLENETWORK AS N

WHERE

O.ID = N.ID

ORDER BY

"FullName" ASC

-----------------------------------------------

SELECT

O.ID, O.FULLNAME, N.ADDRESS

FROM

CGENERICMODBUSOSDIRECT AS O CROSS JOIN CSINGLENETWORK AS N

WHERE

O.ID = N.ID

ORDER BY

"FullName" ASC

Please note that similar queries can be used to generate lists for other drivers. Proper tables for each driver can be found by using the Database Schema. More information on how to use the Database Schema can be found int the manual.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: