How can we help you today?

NBHN125 Installation in NetShelter SX Gen 2

Issue: NetBotz access lock (NBHN125) needs to be installed in NetShelter SX Gen 2 Enclosure

Rack SKU Range: AR3XXXB2 / AR3XXXW2 / AR3XXXSPB2

Cause: NetBotz access lock is compatible with NetShelter SX Gen 2 with single point lock

Resolution:

Refer to the following instruction and video for detailed steps to install NetBotz access lock in NetShelter SX Gen 2 Enclosure

1.Before installing the Handle kit, you must remove the front(handle with locking rod) and rear door handles on your rack.
2.Follow the instruction from the NetBotz handle Kit instruction manual starting from point 2 in page 5.

Schneider Electric Saudi Arabia