Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Calculate the Resistor Value for Open Wire Detection in BMXSDI1602 using DDP 2 or 3 wires?

Issue

Open wire detection in BMXSDI1602 requires to create artificially a leakage current (Ileakage) on the line with a resistor in parallel to the sensor. If this leakage current (0.4 mA < 1.3 mA) is out of range, the external line is considered as cut (or in a short-circuit to ground condition).

Resolution

For a dry contact sensor, set in parallel with the sensor a Rext = 33 K Ω.

However, using DDP 2 or 3 wires, the leakage current needs to fall within the limits defined above. You need to define the value of the resistor (Rext) to set in parallel with the sensor, considering

  • the natural leakage current of the sensor
  • the Rint (internal resistor) of the input, equal to 7.5 K Ω

Then, in order to obtain a current in the range of  :for1

for2

for3

The calculation of Rext is performed with the following formula :

for4

where :

for5